Jul 1, 2023
From directing self-driving cars to accurately predicting the weather to helping doctors identify potential health risks in patients, the feats achieved through artificial intelligence (AI) continue to expand. As AI technologies become further embedded into our daily lives and routines, they are creating a host of new opportunities – including a potentially prosperous one on the horizon for Eaton channel partners.
Generative AI – a type of artificial intelligence technology that can produce content such as high-quality text and graphics in a matter of seconds – has been garnering much hype. If current trends continue, generative AI data center server infrastructure plus operating costs are slated to exceed $76 billion by 2028, according to forecasts by Tirias Research. To put the projection into perspective, that’s more than double the estimated annual operating cost of Amazon’s cloud service AWS, which encompasses one-third of the current cloud infrastructure services market.
Not only is generative AI growing, it’s sparking an upsurge in power requirements
What does all of this mean for Eaton channel partners? Not only is generative AI growing, it’s sparking an upsurge in power requirements – representing a springboard for increased sales of larger UPSs, specifically in edge AI applications.
It’s important to understand that the infrastructure requirements of generative AI are different than that of general-purpose IT applications. Because the innovative capabilities afforded by generative AI require the accelerated processing performance of GPUs, the technology is subsequently bolstering power consumption needs. And that means demand will be increasing for larger uninterruptible power systems (UPSs) and power distribution units (PDUs) able to handle high power and other physical infrastructure solutions. The traditional 5kW per rack will soon turn into 20kW per rack or more.
Even more, the massive power consumption expansion will increase the need for battery back-up systems to help organizations of every size cope with pervasive power outages that are projected to result from the subsequent supply-demand imbalance.
Despite all the hype surrounding generative AI, widespread adoption still looks to be at least two years away, hindered by the need for technology to democratize, security concerns to be alleviated and for costs to drop significantly in order to make business sense for enterprise customers. Looking ahead two years – as AI-ready client devices become widely available and AI on CPUs will drive down costs – we will likely see a hybrid distributed client approach and enterprise customers wishing to own their generative AI infrastructure instead of depending on public cloud providers.
In the meantime, channel partners can expect to begin entertaining interest and questions from customers. Specifying the power infrastructure for 20 kW per rack and up can be complex and requires specific skills. This could be a way for partners to further develop their power practice and add more differentiation, with the help of our support and training teams.
As Eaton is a stronger player in the larger UPS space and we have long supported channel partners with application engineering and face-to-face engagement, this new market trend will put us in an excellent position to help partners increase sales of larger units. As UPSs in the 10-20 kW range become the new norm, we will be here to support you.